Help Prevent Connection Errors in Multiple Port Systems
Help ensure that each fluid line is connected to the correct port, preventing misprocessing of tests and potential damage to the equipment with IdentiQuik. Before a physical connection is made, the RFID reader -- which is integrated into the CPC IdentiQuik connector -- reads the tag and tells the control unit what is being connected to the instrument port. If a misconnection is attempted, the control unit can display an error message, trigger an alarm; or shut down the equipment until the error is corrected.
Provide Correct Operational Settings
Once the identification data on the tag -- which is integrated with the IdentiQuik RFID-enabled connector -- has been read, the control unit automatically sets parameters such as pressure, flow rate, and operating time to match the requirements for the media that has been connected. Operational control settings reduce the risk of human error when setting operating variables -- preventing harm to the equipment and eliminating the risk of invalidated tests.
Enforce Required Limits on Fluid Chemical Usage
The controller tells the wireless IdentiQuik RFID-enabled connector to write to the tag on the consumable product each time the product is used. If it is a limited use consumable, the controller keeps track of the usage and will not allow a test to be processed once the threshold is reached. This prevents testing from being performed with potentially outdated media.
IdentiQuik Validates Connected Media
CPC's intelligent IdentiQuik connectors alert manufacturers and service providers that OEM-supplied consumable products are being used on the equipment, device or test instrument. The reader in the CPC smart connector reads the identification data on the consumable package and verifies that inferior or incorrect media is not being connected. This prevents potential damage to the instrument and provides brand protection for proprietary reagent solutions.
Monitor Consumption of Media with Smart IdentiQuik
RFID-enabled IdentiQuik connectors can monitor the amount of media used in a fluid dispensing application. The amount of media required for each use is specified in the control settings of the device. Each container contains an RFID tag that is programmed with the initial volume of media. As the media is consumed the controller writes to the consumable product tag and deducts the amount of media used for each connected line. When a container is close to empty, the control unit will alert the operator that additional media is required before the next use can be started.