Two-Phase Immersion Cooling

    Use Our Product Specifier

    Systems Need Info Now!

    With more and more information being accumulated, processed and stored digitally, the expectation is that access to the massive amounts of data should be practically instantaneous. Application demands are driving increased deployments of high-performance computers as well as accelerated implementation of cloud and edge computing infrastructures. Data centers professionals are continually asked to provide faster data delivery, better efficiency and increased cost effectiveness in a more sustainable way.

    Not Able to Keep Up

    Traditional data centers use air cooling methods that are known to be inefficient at dissipating heat. There is a limit to how much cold air can be blown into or how much hot air can be sucked out of racks in a data center facility before needing to space them out. This leads to larger footprints and sidesteps the problem of air cooling inefficiency instead of facing it straight on.

    Issues Facing Data Center Professionals

    • Efficient use of space
    • More limited optimal locations for large data centers
    • Pressure for increased use of sustainable technologies
    • Power usage effectiveness (PUE) goals
    • Increasing demand for smaller data centers at the Edge
    • Continued speed of technology innovation 

    Use CPC Liquid Cooling Quick Disconnects for Two-Phase Immersion Cooling

    Collaborating with thermal engineers, system designers and data center operators around the world, CPC is fully engaged in understanding the challenges and requirements of two-phase immersion cooling. We are familiar with the materials and chemistry that thermal management professionals design for, including the various fluids used in 2PLIC and its effects on other components within a system. CPC’s purpose-built Everis® quick disconnect couplings and connectors (QDs) portfolio for use in the liquid cooling systems is the result of years of working with thermal management professionals and learning what they require as they design liquid cooling systems for a wide variety of computing environments.

    The Larger the Data Center, The Bigger the Need for New Cooling Methods

    Exceptionally large data centers, which can occupy hundreds of thousands of acres and can use more than 205 terawatt-hours of electricity, are looking for solutions that provide computing at higher densities and deliver results that:

    • Enable space reduction
    • Increase efficiency
    • Reduce costs
    • Allow for sustainable operations
    • Permit future technology innovations

    Two-Phase Liquid Immersion Cooling: An Up-and-Coming Solution

    Two-phase liquid immersion cooling (2PLIC) is the latest advancement in liquid cooling. Similar to single-phase immersion cooling, electronic components are submerged into a dielectric liquid. However, the immersion fluids used by two-phase liquid cooling are vastly different from those used in single-phase cooling. During two-phase immersion cooling, the immersion fluid absorbs the heat and begins to boil. The fluid then turns into a vapor that rises and condenses on a heat exchanger (condenser) within the immersion tank. The condenser transfers the heat to facility water for waste heat recovery where it can be used as warm water in the facility, for example.

    Why Choose Two-Phase Immersion Cooling?

    The two-phase immersion cooling fluid is completely contained; there is no loss of any fluid during operation.

    Benefits of 2PLIC

    • Less cooling infrastructure required
    • Lower―even zero―water usage
    • Reduced square footage needed
    • Lower PUE with more energy available for computing
    • Overall higher efficiencies

    "Most 2PLIC systems operate at a full system (not just a mechanical system) PUE of 1.028, meaning less than 3% of energy is used on cooling infrastructure, leaving 97% available for computing."

    Resource: https://www.missioncriticalmagazine.com/articles/92948-two-phase-liquid-immersion-cooling-enables-the-future-of-technology

    Getting Ready to Implement

    Currently only a few companies are able to implement data center platforms using 2PLIC technology and its associated engineered fluids. IT hardware that supports two-phase immersion cooling is not readily available. However, data center professionals and thermal engineers are educating themselves on the technology and the potential positive impact it could have on their businesses. Once the hardware is readily available, an increasing number of data centers of all sizes may jump on board to take advantage of the benefits of two-phase liquid immersion cooling.

    Everis Quick Disconnects Engineered for Liquid Cooling

    Trusted Reliability

    Everis’ range of seal options and QD materials are engineered to meet the temperature, chemical and pressure compatibility requirements of today’s liquid cooling systems. You can count on Everis connectors to withstand side load and tensile pressures during installation and endure long periods of connection with leak-free reliability.

    Dependable Durability

    CPC provides a wide range of high-performance quick disconnect couplings that deliver years of leak-free performance. Engineered for the rigors of today’s data center computing environments, Everis non-spill connectors deliver optimized flow rates with excellent flow-to-size ratio for superior performance. CPC Everis quick connects feature a valve design that is precision engineered for extended connection time and is compatible with a wide variety of liquid cooling fluids, including dielectric and inhibited glycol fluids.

    Maximum Control

    Make the choice that’s right for you from a wide array of liquid cooling QD designs. CPC Everis QDs come in an expanding variety of sizes, termination options and materials including plated brass, aluminum, stainless steel, high-performance polymers. Configurations include blind mate, latched, straight and elbow connectors with seal options including EPDM, FKM and Viton®. Where space is an issue, there’s Everis blind mate or swivel joint QDs. They are perfect configurations for manifold and chassis system designs or unique arrangements that feature tight spaces.

    Expert Flexibility

    The key to effective design for liquid cooling is accurately determining fluid handling requirements early in the design process. With application engineers who drill into the details, CPC is able to offer insights as thermal engineers test and validate performance and fit for the liquid cooling technology solutions that work best with their liquid cooling server rack environment. All Everis liquid cooling QD solution designs are rigorously tested ─ including materials testing, product testing and torture testing to failure ─ to meet product design specifications. As a matter of fact, CPC offers reliable, reproducible performance and provides validation reports that support the QD’s performance attributes.

    Straightforward Serviceability

    When your systems are due for scheduled maintenance, CPC's latched Everis connectors are designed for ease in liquid cooling system serviceability, including drip-free non-spill disconnections for safer and quicker upkeep or repair. The simple-to-use thumb latch provides both ease and speed of installation and system maintenance. Cold plate liquid cooling systems may also use Everis blind mate or swivel joint QD configurations for manifold and chassis system designs or unique arrangements that feature tight spaces.

    Connection Assurance

    With a sleek body and ergonomically designed thumb latch, Everis liquid cooling connectors deliver single-handed operation along with the audible CPC click to assure technicians to know they’re connected. And, Everis Series’ low force to connect makes it simple to ensure a complete connection.

    Ready to see the line-up of CPC liquid cooling QD connectors? Visit our Products.

    Technical Insight from CPC's Liquid Cooling Fluid Handling Engineers

    Helpful Information for Selecting CPC QDs for Liquid Immersion Cooling