• 寻找代理商

在线工具

产品规格 确定用于您特定项目的接头类型
CAD 下载 下载特定接头的 CAD 图纸,以直接用于您的设计软件
    产品目录 技术参数表 使用我们的产品目录,查看完整的产品列表
    产品目录 技术参数表

    6 Traits of Non-Spill

    How quick disconnect couplings evolved for low-pressure fluid handling

    Once the domain of high-pressure hydraulics, non-spill performance is now available in quick disconnect solutions for low-pressure fluid handling in countless products and processes.

    The term non-spill, when discussing couplings, describes a specific type of connector meant to reduce spillage to near zero whenever couplings are disconnected. This is often achieved through the design of the valves housed within the coupling body. Originally designed as heavy-duty metal couplings for high-pressure, industrial hydraulic applications, non-spill has evolved into a category of plastic and metal connectors suitable for a wide variety of fluid-handling applications requiring minimal spillage and air inclusion.

    Defining Non-Spill Fluid Handling Technology Terminology

    For the purposes of this white paper and non-spill technology discussions, the following terminology is frequently used. As with any technical subject matter, it is important to understand and use common reference terminology.

    Spillage. The volume of liquid between the valve faces released every time the coupler is disconnected. One drop of water = .05 ml. A traditional valved 3/8” coupler has ~ 1–3 ml or more spillage per connection cycle; CPC non-spill technology reduces this volume to .01–.03 ml spillage per connection cycle with the same 3/8” flow area, at low pressures.

    Inclusion. The volume of air put into a system every time the coupler is connected. A traditional valved 3/8” coupler has ~ 2 ml or more inclusion per connection cycle; CPC non-spill technology reduces this volume to ~ 0.4 ml inclusion per connection cycle with the same 3/8” flow area.

    Leakage. Media that leaks out of the coupler while connected or disconnected. In a well-designed connector, regardless of its spillage volume specifications, there should be no leakage.

    Flow Area. The areas through which the fluid or gas media travel. Used to specify coupling size to meet requirements of tubing size, pressure drop, flow rate, etc.

    Low-Pressure Non-Spill Fluid Handling Technology Evolution

    The original non-spill quick disconnects for high-pressure applications were ball and sleeve coupler packages made from machined brass, zinc-plated steel, stainless steel and aluminum. Because of the high pressures common in hydraulic applications — up to 15,000 psi (1,030 bar) — metals were the only logical material to contain such pressures. Plastic materials came into use because they provide the strength required for lower-pressure applications. Plastics reduce the cost and weight of couplings and answer concerns related to chemical compatibility.

    From a design perspective, the traditional characteristics of a non-spill quick disconnect coupling include a flush-face valve design, metal construction and the ability to withstand high pressure ratings. The flush face valve design minimizes the amount of spillage each time they are disconnected, thus the reference as a non-spill connector. This reduced spillage is key to maintaining a clean environment, containing harmful fluids and protecting workers.

    For some time, low-pressure fluid-handling applications have utilized non-spill quick disconnects originally designed for high-pressure environments. However, as more low-pressure uses for non-spill connectors emerged, it became clear that high-pressure couplings were over-engineered — and certainly costly — for connecting flexible, semi-rigid and reinforced tubing in low-pressure applications. To precisely meet the non-spill requirements of low-pressure fluid applications, a new category of couplings has evolved: low-pressure, small footprint thermoplastic and metal quick disconnect couplings that maintain non-spill performance characteristics.

    Six Traits of Evolutionary Design in Non-Spill Couplings

    The following six traits describe the evolution of the non-spill coupling tailored for low-pressure environments.

    Evolutionary trait #1: Maintenance of flush-faced valves

    The design of non-spill valve technology is not new; what is new is the migration of the flush-faced valve to connectors for flexible tubing used in low-pressure applications.

    Connecting and disconnecting in low-pressure environments was historically accomplished with a poppet-style valve. This valve style traps liquid in the valve cavity on the external side of the valve seal. Though the valve has shut off the flow, this remaining volume of fluid can “spill” from the coupling.

    Figure #1: Poppet Valves

    In contrast, the flush-face valve, due to its design, allows no more than a coating of liquid on the valve surfaces, thereby nearly eliminating spillage and ensuring repeated dripless connections and disconnections. Inclusion, or the air put into the fluid system during every connection, is also drastically reduced with flush-face valve design. The benefits of near-zero spillage and inclusion have become important in many applications, from medical devices and equipment to chemical handling.

     Figure #2: Flushed Faced Valves

    Evolutionary trait #2: Switch from metal to engineered polymers

    Metal housings and internal valves were originally chosen for non-spill couplings due to the pressure demands of hydraulic applications. Low-pressure environments do not necessarily require the performance attributes of metal housings and internal valves. Design engineers looking only at metal high-pressure coupling alternatives may be limited in the available selection of weight, package size, flow performance and, in particular, cost. Stainless steel offers the widest chemical compatibility but is also the most expensive metal choice.

    As an alternative, engineered polymers have gained a substantial foothold in applications where metal had been the industry standard. Reduced weight, high strength and rigidity, and the ability to achieve complex part geometries are all benefits of engineered polymers. Choosing polymer couplers can provide savings of 50 to 75% compared to metal disconnect products. Some non-spill couplings also incorporate a soft-touch over-mold for superior ergonomics and color coding. Others feature a glass-filled polypropylene body that offers chemical resistance and increased durability.

    Figure #3: NS4 colorsFigure #4: NSHD body and insert

    Evolutionary trait #3: Low-pressure environments, minimal pressure drop

    In low-pressure fluid handling applications, systems typically operate in the pressure range of vacuum to 120 psi (83 bar). The use of non-spill quick disconnects designed for applications operating in the 10,000 psi range is overkill.

    A quick disconnect designed specifically for low-pressure fluid handling applications can deliver all the desirable features of low spillage, low air inclusion and minimal pressure drop. Low-pressure quick disconnects provide higher flow and lower pressure drop compared to their metal counterparts by leveraging the design flexibility gained through the use of plastics and advanced manufacturing techniques, as well as their efficient, high-flow valve design.

    Evolutionary trait #4: Compact design

    Many low-pressure applications requiring a non-spill coupling also demand a compact design, due to both smaller diameter tubing sizes and the interior or hard-to-access locations where many non-spill couplings are applied. For instance, non-spill couplers used in server racks for liquid cooling or inside in vitro diagnostic equipment need to be as compact as possible to minimize product real estate used and to allow room for technicians to connect and disconnect the couplers.

    Today’s increasingly compact couplings are achieved partially through the internal design of the coupling. Some manufacturers provide non-spill couplings that can connect tubing with an inside diameter as small as 1/16” or less.

    Figure #5: NS1 body and insert

    Evolutionary trait #5: Ease of use

    An enduring characteristic of high-pressure couplings is the physical difficulty users can have in connecting and disconnecting the couplers. When connecting the couplers, the process can require significant amounts of force. This user inconvenience is addressed in the design of some low-pressure quick disconnects with the introduction of an ergonomic thumb latch that makes the process of disconnecting much easier.

    Another user benefit provided by some new non-spill connectors is an audible “click” that sounds when a secure connection is made.

    Evolutionary trait #6: Chemical compatibility

    For certain low-pressure fluid-handling applications, the chemical compatibility of the fluid and the connector or its parts needs to be considered. Unlike hydraulic applications — where fluid and metal do not react with each other — low-pressure fluid-handling applications can involve media that reacts with metal.

    To address this potential concern, connector designers use polypropylene (which offers chemical resistance to many fluids) or other engineered thermoplastics. Some applications also require a metal-free flow path. One method to achieve this is to isolate the springs from the flow path through the use of an O-ring. This ensures a degree of separation between the fluid and any metal. The O-ring seals separate fluid flow from the valve actuation springs, thereby ensuring high-purity flow paths well suited to applications such as semiconductor manufacturing. In some non-spill couplings, coated springs give a second degree of separation between fluid and metal.

    Industry Uses of Low-Pressure Non-Spill Couplers

    There are many real-world uses of the non-spill connectors that have evolved from their high-pressure origins. Below are a few examples:

    Medical devices and in vitro diagnostic equipment

    Many fluid handling applications for medical devices require minimal air inclusion for accuracy and procedural efficacy. Some devices also require the ability to disconnect tubing without drips or spillage to prevent contact with hazardous fluids and to maintain a safe and clean environment. Analytical equipment used for diagnostics in laboratory or patient care facilities require the same drip-free disconnect to maintain media integrity, prevent contact with biohazards and maintain a safe working environment.

    Ink management

    Whether ink is water-based, solvent-based or UV curable, any spillage is a problem. Like water-based inks, solvent-based inks leave a mess but can also have noxious fumes. Because UV inks only dry under exposure to UV light, small spills wiped up with rags continue to stay wet long after cleanup. Non-spill connectors help keep ink in the system — eliminating the mess at the source — so ink never comes into contact with users or equipment components.

    Liquid cooling of electronics

    Non-spill couplings are ideal for use in liquid cooling applications. By reducing spillage of water or coolant to near zero, server rack technicians can confidently connect and disconnect couplings without fear of drips that can damage or destroy equipment. Color coding helps prevent misconnection between hot and cold lines. The latest design features ensure long-term functionality that accommodates prolonged static connections.

    Figure #6: LC bodies and inserts

    The State of Non-Spill Quick Disconnects for Low-Pressure Applications Today

    The range of non-spill quick disconnects for low-pressure applications continues to grow, from glass-filled polypropylene couplings in increasingly small package sizes to chrome-plated brass non-spills specifically designed for liquid cooling applications.

    The preceding six evolutionary traits explain why and how today’s non-spill couplings have been designed to meet the unique requirements of low-pressure fluid-handling environments.

    What started as a high-pressure non-spill coupling has expanded beyond the scope of hydraulics to bring non-spill performance to many industries — and very likely, to products of the future taking shape on CAD program screens today.

    Figure #7: Non-spill family disconnected

    Back to Top